Understand faces and people's motions: OMRON's Image Sensing technology OKAO™ Vision
OKAO™ Vision Functions
Technology

Hand Gesture Recognition and Hand Detection
Recognize hand position and movement from the camera image.
It realizes user interface by natural operation with various devices.
Initialization is not required with Image Sensing technology
Can realize a more natural recognition
by using the relation between the position and orientation of the face and hand.

Initialization is not required with Image Sensing technology
Detects the palm from the images taken with the camera.
It corresponds to "up, down, left, and right" movements which can be instructed easily.

Can cover large distances.

Can be used with web cameras, built-in cameras, digital cameras, etc.
Can be usd on various devices like computers (Windows and Mac),
smartphones (Android, etc.), tablets, digital cameras, etc.

Functions
Motions
Up, Down, Left, Right

※Support for additional motions and gestures is planned.
Shape
Palm

Position
Coordinates of the hand.

Applications
For smartphones
e-book viewer

For televisions
Remote control

※Microsoft and Windows are either registered trademarks or trademarks of Microsoft Corporation in the United States and/or other countries.
※Android is a trademark of Google Inc.
※Other product or service names are either registered trademarks or trademarks of their respective companies.