Detect people's location to optimize comfort and energy saving.
Don't you think that using air conditioner for the whole office is a waste of electricity when working only in small area of the large room?
Monitor the location and grasp the number of people when Human Body Detection of Image Sensing technology is implemented. Then adjust the temperature when necessary. This can be used for lighting apparatus or BGM settings too.
This enables to keep the comfortable environment from people's condition in medical or nursing facilities without the constantly turn on or off devices.
Saving energy of public facilities such as offices, exhibitions, libraries, department stores or schools means significant cost reduction.