This page may not be properly displayed depending on the browser used. We recommend using the following browsers in order to view this site: Internet Explorer 7.0 or later, Firefox, Chrome, Safari (newest version of each)(note that the page may still not be properly displayed depending on the settings used).
Detect the location and number of people in large office.
Adjust temperature and lightning of only necessary places.
If it is used for systems such as building automations, it'll contribute to significant energy savings and cost reduction.
A great smile can lead to better customer satisfaction.
Rate one's own smile with Smile Degree Estimation and If it is used for emproyee training, the quality of hospitality and services can be improved.
Obtain information about the customers automatically
such as age, sex and the number.
The comparison of daily data enables marketing
along the exact needs of each store.
Now on saleHuman Vision Components(HVC-P2) B5T-007001
Incorporates multiple Image Sensing algorithms and a camera module into a compact configuration. Board type component easy to install on equipment.